ProductsInterfaceSupportFAQ

Frequently asked questions

Video SerDes Feature FAQ

Q How does the PTN3700 achieve low electromagnetic emission?
A The PTN3700 uses 1, 2, or 3 pairs of differential subLVDS high-speed serial lanes, along with a differential pair for clock. The low voltage differential swing of 150mV is meant to reduce electromagnetic emission. The combination of low voltage swing, differential signaling, and low intra-pair skew ensures that the already small electromagnetic emissions are effectively canceling themselves out. Furthermore, the slew rate-controlled parallel CMOS output circuitry of PTN3700 (when used in receiver mode) is yet another feature of PTN3700 to ensure low electromagnetic emission.
Q How small is the PTN3700 package?
A The PTN3700 is offered in a tiny VFBGA package of 4 x 4.5mm, with a maximum height of 1mm and ball pitch of 0.5mm. When used as a receiver, the PTN3700 is also offered as an even smaller gold-bumped bare die, which can be mounted on glass of the display unit.
Q What is frame mixing? Where can frame mixing be useful?
A The PTN3700 receiver implements frame mixing, which is a proprietary pixel-mapping algorithm that features the ability to render full 24-bit color resolution using a cheaper 18-bit display. Provided that the input serial data to the PTN3700 receiver contains 24-bit RGB data, the frame-mixing mode of PTN3700 converts 24-bit RGB input to 18-bit output to the display by modulating the LSB (Least Significant Bits) to give the viewer the visual effect of a 24-bit display. The frame-mixing algorithm is especially effective for still pictures with subtle color gradations. It is worthwhile to note that the algorithm does not degrade the viewer's perception of moving pictures.

Other Questions

If you have other questions that you would like answered, please contact us.
Standard ICs quick find
Standard ICs sections
See also