| Q |
How long is the link length that PTN3700 is able to support? |
| A |
This significantly depends on the properties of the link medium (including connectors, launches, and PCB) such as loss per unit length over frequency, noise susceptibility of the medium, as well as the degree to which skew between data and clock lanes can be managed.
Frequency of operation is also a factor.
However, the PTN3700 has been proven to effectively drive up to 25cm of typical flex foil cable in laboratory evaluations.
For specific use cases that require lengthy serial interconnect, please contact Interface.Support@NXP.com.
|