ProductsInterfaceSupportFAQ

Frequently asked questions

PCI Express PHY Compliance and Interoperability FAQ

Q What are the differences between the PX1011A and PX1011B?
A The PX1011B is an improved version of the PX1011A and is 100% PCB and functionality backwards-compatible with the PX1011A. The main differences between the PX1011A and PX1011B are:
  • Improved power supply range
  • Improved transmit jitter performance
  • Improved receiver sensitivity
Q Can existing PX1011A and PX1012A customers use the PX1011B without doing a redesign of their PCB?
A Yes, definitely. In fact, because of the better performance of the PX1011B versus the PX1011A and PX1012A, we encourage customers to immediately switch to the PX1011B. Because of the more relaxed VDDD3 and VDDA1 supply voltage requirements, customer PCBs designed with the PX1011B in mind can potentially be simpler than earlier PCBs designed for the PX1011A and PX1012A. Even if the customer does not care about simplifying the power supply circuit, existing PCBs using the PX1011A or PX1012A can immediately use the PX1011B without any adverse impact. There is no need to redesign the PCB.
Q Is the PX1011B v1.0a- or v1.1-compliant?
A The PX1011B is both v1.0a- and v1.1-compliant.
Q Are the PX1011A and PX1012A on the PCI-SIG Integrators List?
A The PX1011A is listed on the PCI-SIG Integrators List since July 2005. The PX1012A has passed PCI-SIG compliance tests with the PLDA PCI Express PXPIPE EZ IP Core in December 2005.
Q Is the PX1011B on the PCI-SIG Integrators List?
A Yes. Since January 2008, the PX1011B is listed on the PCI-SIG Integrators List.
Q Have the PX1011A and PX1012A participated in previous PCI-SIG plugfests?
A The PX1011A participated and passed in various PCI-SIG Plugfests (#45, #48, #49, #53). At the PCI-SIG #53 Plugfest in December 2006, the v1.1 compliance tests became available officially, and the PX1011A passed all the official v1.1 electrical tests, and interoperated successfully with other devices. The PX1012A passed both v1.0a gold and informational v1.1 jitter tests at PCI-SIG #48 Plugfest in December 2005.
Q Are the PX1011A/B interoperable with PC systems from various vendors?
A
Yes. Both the PX1011A and PX1011B have been extensively tested in mulitple PC systems by NXP Semiconductors with partners and customers. Both devices participated in multiple PCI-SIG Plugfests with successful interoperability results.
PC Systems Tested by NXP Semiconductors and Partners
  • Abit KN8 SLI (Nvidia nForce4 SLI chipset)
  • Apple MAC G5
  • Asrock 775TWINS-HDTV-M-ASR (ATI Radeon Xpress 20, Uli 1573 chipset)
  • ASUS A8N32-SLI Deluxe x16 slot (nVidia nForce4 SLI chipset)
  • ASUS A8NE (x16, two x1 and one x4 slots)
  • ASUS M2NPV-VM (x1 and x16 slots)
  • ASUS P5GP motherboard (Intel 915G chipset)
  • ASUS P5LD2 DELUXE (Intel i945 chipset)
  • ATI Radeon RS485 chipset
  • ATI RS600 mobile chipset
  • Dell Dimension 4700 x1 and x16 slots (Intel 915G chipset)
  • Dell Dimension 8400 (Intel 925G chipset)
  • Dell Dimension 9100 (Intel 945P chipset)
  • Dell Optiplex GX280 x1 slot (Intel 82915G and ICH6R)
  • Dell PowerEdge SC430
  • Dell Precision 370 x1 slot (Intel 925X Express chipset)
  • Dell Precision 380 x1 and x4 and x16 slots (Intel 955X Express chipset)
  • Dell Precision 470 x8 slots (Intel Turnwater E7525 chipset)
  • Dell Precision 670 workstation
  • ECS Elitegroup RS-400-A 2 x1 slots (ATI RS400/SB400 chipset)
  • Freescale MPC8548CDS (x4 slot)
  • Gigabyte GA-81915G Pro (Intel 915G chipset)
  • Gigabyte GA-G1975X 2 x 16 and 2 x4 slots (Intel 975X chipset)
  • HP dc7600 (Intel 945G/P chipset)
  • HP Proliant Server (Intel Blackford chipset)
  • HP XW4200
  • HP XW4300
  • IBM 8113-F8U
  • Intel 915G chipset
  • Intel 915GEV (x1 slot)
  • Intel Alcolu (Intel Blackford chipset)
  • Intel Alviso 915P chipset
  • Intel Blackford 5000P chipset
  • Intel D925XCV all slots (Intel 925x ICH6)
  • Intel D955XBK Motherboard
  • Intel E8500 chipset
  • Intel Greencreek 5000X chipset
  • Intel Harwich 800+ (Intel Twincastle E8500 chipset)
  • Nvidia MCP65 chipset
  • Intel PDK System Rev B
  • Intel PDK System Rev C
  • Intel Lindenhurst x16 slot (E7520 chipset)
  • Intel StarLake (Intel Blackford chipset)
  • Intel Tappen 945G chipset
  • Intel XW8400 (Intel Greencreek 5000x chipset)
  • MPC8548 CDS
  • MSI (Intel i915 chipset)
  • Nvidia 6150 (x1 slot)
  • NVidia MCP55 (ASPM on)
  • Nvidia MCP67D chipset
  • NVidia nForce4 Ultra
  • PLX8532 on Dell Prevision (x16 slot)
  • Serverworks GC-SL
  • Shuttle ATI Express 200 chipset
  • Supermicro PDSGE (x1 slot)
  • Supermicro X6DA8G (x16 and x4 slots)
  • Supermicro X6DAE-G all slots (Intel E7525 Turnwater chipset)
  • Supermicro X6DAE-G2 Expansion chassis all slots (Intel SE7525 cabled PCI Express)
  • Supermicro x6dvl-eg2 (Intel 915 / 945 chipsets)
  • Supermicro X6DHE-G2 (x8 slot)
  • Tyan K8WE S2895 x1 and x16 slots
  • Tyan S2895 Thunder K8WE (nVidia nForce Professional 2200 and nForce Professional 2050 chipsets)
Other PC Systems Tested at PCI-SIG Plugfests
  • Allion (Intel 915 chipset)
  • ATI RD580 Motherboard
  • HP 570G3
  • HP Blackford Server
  • HP E8500 Server
  • HP Greencreek Workstation
  • Intel Broadwater Motherboard
  • Intel Twincastle Motherboard
  • Nvidia Motherboard (C51 chipset)
  • SUN Sparc Fireball
  • ULi M1695 Motherboard

Other Questions

If you have other questions that you would like answered, please contact us.
Standard ICs quick find
Interface sections
See also