ProductsInterfaceSupportFAQ

Frequently asked questions

Industrial UART Baud Rate Generation FAQ

Q What is the highest baud rate produced by an internal clock?
A The highest baud rate is an X1 clock input divided by 16. For example:
At 3.6864Mhz, the highest baud rate is 3.6864M/16 = 230.4K baud.
At 8Mhz, the highest baud rate is 8M/16 = 500K baud.
Q What is the maximum baud rate in timer mode with a crystal of 3.6864Mhz?
A The maximum baud rate is a C/T clock input divided by 64. For example, at 3.6864Mhz, the maximum baud rate is 3.6864M/(2*16*2) = 57.6K baud.
Q If the crystal of 3.6864Mhz is doubled, will the baud rates in each column in the baud rate selection table be doubled?
A Yes. For example, if a crystal of 7.3728Mhz (2*3.6864Mhz) is used, the baud rates will be doubled as follows: The 57.6K and 115.2K in one column will become 115.2K and 230.4K.

Other Questions

If you have other questions that you would like answered, please contact us.
Standard ICs quick find
Interface sections
See also