![]() |
|||||||||||||||||||||||||||||||||||||||||||||||
|
|||||||||||||||||||||||||||||||||||||||||||||||
NXP PCA9633 demo boardIntroduction
4-Bit LED Controller Demo Board Offers Easy LED Dimming and Blinking
The PCA9633 Demo Board demonstrates the new PCA9633 Fast-mode Plus (Fm+) 4-bit I2C LED controller.
Red, Blue, Green, and Amber LEDs are connected to the PCA9633 and, through individual pulse width modulation (PWM) of each LED, show different levels of intensity and color mixing.
The preprogrammed microcontroller supports six different modes of operation including color wash and random color and is user reprogrammable for endless variations of functionality and experimentation.
![]() Highlights
Contents
PCA9533 Demo Board
The PCA9633 demo board contains a
NXP P89LPC925 microcontroller which controls a PCA9633 I2C LED driver/RGBA mixer.
The demo board also contains a P82B96 I2C bus buffer so that the microcontroller can operate over the higher-drive Fast-mode Plus I2C-bus.
A 4-key keypad is included for operator control of the RGBA color mixing and light patterns.
P89LPC925
The 80C51-based microcontroller controls the PCA9633 with embedded firmware.
The user can edit this code and reprogram the flash microcontroller via a 10-pin header using any external ICP style programmer.
PCA9633
The 4-bit I2C-bus LED controller has individual 8-bit 256-step PWMs for each LED color and a 5th 8-bit 256-step PWM to either dim or blink the combined color.
P82B96
The bus buffer allows the microcontroller to operate with the PCA9633 on the higher drive Fast Mode Plus I2C-bus and operation off the board.
![]() Uses
Four LEDs are connected to the PCA9633 and, using pulse width modulation (PWM) of each LED, multiple different intensity levels are available for color mixing.
To use the demoboard, push DIP Switch SW8 to the ON position.
The LEDs will immediately flash and glow.
To select a different mode of operation, press the MODE button (PB1).
The LED will flash amber a number of times to denote which mode was entered.
Use the other 3 buttons (SELECT, PLUS, and MINUS) to change the settings.
Six different modes of operation are provided and described below:
Mode 1: Auto Demonstration Mode
Automatically selected at start up.
The LED first shows Mode 2 for 10 seconds, then shows Mode 3 for 10 seconds, and then repeats.
Mode 2: Color Wash Mode
Goes through blends of different colors continuous.
Mode 3: Random Color Mode
Randomly shows different colors without blending transitions.
Mode 4: User Color Mode
Allows the user to choose a color by selecting the amount of each LED's PWM output as well as the 5th group PWM that is used to dim or blink the combined colors at the same time.
Mode 5: Multiple Card Chase Mode
Uses multiple cards and the group call feature of the PCA9633 to generate a chase pattern of 2 (yellow/red), 3 (yellow/red/green), or 4 (yellow/red/green/blue) colors for up to 8 boards (master plus seven slave boards) connected via the RJ45 jacks.
![]() Mode 6: Output Enable Control Mode
Demonstrates the Output Enable control pin input that Hi-Zs the LED outputs.
This mode changes the LED diffuser color to purple and blinks all LEDs at the same rate.
Products
Support
DocumentsOrdering Information
Part Number OM6276: NXP PCA9633 Demo Board
The demo board can be purchased from authorized distributors:
Programming the Microcontroller
The USB-ICP-LPC9xx In-Circuit Programmer, Flash Magic, and Source Code is needed if you want to be able to reprogram the microcontroller used on the PCA9633 demoboard to make your own color changing patterns.
USB-ICP-LPC9xx In-Circuit Programmer
Flash Magic
Flash Magic can be obtained from Embedded Systems Academy.
This software can be used to load the microcontroller with compiled hex files.
Please visit http://www.esacademy.com/software/flashmagic/ for more information, release notes, application notes, and to obtain the software.
Flash Magic is sponsored by NXP Semiconductors.
Source Code
Technical Support
Contact Sales@TeamFDI.com or NXP Semiconductors depending on where you obtained you PCA9633 demo board.
More Information
Literature
Links
|
|||||||||||||||||||||||||||||||||||||||||||||||