ProductsMicrocontrollersSupportMicrocontrollers Design Examples

Point Of Sale (POS) design example

Description
This is a demonstration-only design of a Point Of Sale (POS) system using the NXP LPC2214FBD144. Fiscal Cash Register (FCR) is a kind of POS machine which is popularized by governments, in particular, in China. A tax control function is added to the POS machine for revenue supervision. Considering the national standard and function expansion and complexity, an ARM MCU is used in the application market. The LPC2214 is the central control unit of the system. The system consists of an LCD, NAND flash, keypad, printer, RTC, IC card, etc. The FCR demonstration system is divided into two boards. The first is the NXP LPC22xx development board. On this board, general peripheral resources are integrated such as external flash and SRAM, keypad, ethernet, LCD, USB, CF card, and IDE. This can be considered as the motherboard used for the overall application. The FCR-specific resources such as NAND flash, UART, printer, and IC card are on the extended board. If more resources are needed, just replace the extended board. In the system, the LCD module is needed to display the operation and the keypad is used to send commands to the system. NAND flash is used to store the business data and the DOT Matrix printer is used to print the invoice. The IC card is used for security. The POS demo system demonstrates the functions which are important in a complete FCR system. The demo system can be used for software development and can help in reducing the development cycles and time to market.

Block Diagram

Products
Below are recommended microcontrollers for use in implementing this design to a system.

MCUs

Click for datasheet. Also, see datasheet disclaimer.
, , indicate product status. Click or for more or less detail.
 LPC2214 Microcontroller with 256KB ISP/IAP flash, 10-bit ADC, external memory interface
LPC2214FBD144LQFP-144DiscontinuedSOT486-1Pb-FreeMSL=2
LPC2214FBD144/00LQFP-144DiscontinuedSOT486-1Pb-Free        
LPC2214FBD144/01LQFP-144ProductionSOT486-1Pb-Free        
Family Functions Literature Support Docs Tools Consultants Price Buy Online More...
More Information

Images


Working Prototype

Schematics

Example Code

Disclaimer

This design example shows possible hardware and software techniques used to implement the design. It is imperative that the viewer use sound engineering judgment in determining the fitness of this design example for any particular application. This design example may include information from 3rd parties and/or information which may require further licensing or otherwise. Additional hardware or software design may be required. NXP Semiconductors does not support or warrant this information for any purpose other than an informational design example.
Standard ICs quick find
Microcontrollers sections
See also