![]() |
||||
|
||||
ConsultantsContact
ZLG
China
Locations
China
Applications
Auto/Transport, Consumer, Industrial, Power, Process Control, Security, Telecom, White Goods
We provide a completed and supply guaranteed system for our customers.
We provide a full range of technical support throughout the product life and guarantee each pie of the supply chain.
Our service ranges from individual technical supports to full series hardware and software designs.
We respect our customers' requirements, and help them solve their practical problems.
We are capable to provide full solutions on hardware and software designs based on customer requirements; also we can provide a specific software programming together with the hardware configuration peripherals.
According the customer requirements, we can provide a full set of hardware together with documentations, such as a set of controller's board with tutorial materials and experiment information.
We can supply low-level hardware or software protocols, source codes, types of development tools, and basically any services and supports that related to the
NXP microcontroller and embedded products.
Products
Microcontrollers
The following
NXP products are supported:
Demonstration and Evaluation Boards
The following products are either developed by or supported by the consultant:
The EasyARM2200 Development tool is a powerful development board for ARM 32-bit microcontroller.
It uses the
NXP LPC2210 processor, an ARM7TDMI-S core, opened-bus microcontroller, and with JTAG debuggers function.
It provides the keyboard, LEDs, RS232, and other common functional peripherals.
It also contains several interfaces, such as IDE hard disk interface, CF memory Card interface, Ethernet interface, and modem interface.
More Information
Background
ZLG has 248 engineers, focused on selling, development, promotion and technical support of microcontroller applications and embedded systems' products, specializing in electronic product developments and applications.
We cover the fields of embedded system tutorial equipment, electronic equipment, industrial communications, microcontroller development tools, automotive electronics, and intelligent water and power meters.
Our company provides strong technical power and the capability for massive production, which, combined with our extensive sales network within China, make ZLG the market leader in embedded products in mainland China.
Disclaimer
NXP Semiconductors provides consultant information in an effort to support its customers through independent 3rd parties.
NXP believes that the information presented herein is fair and accurate.
NXP does not endorse or warrant a listed consultant's fitness for any particular purpose.
You should contact the consultant directly to discuss your particular needs.
|
||||