ProductsStandard ICsSupportConsultants

Consultants

Contact
Sandring Systementwicklung
Sten Sandring, Dipl.-Ing.(FH)
Systementwicklung und -programmierung
Wollersdorf 13
D-91564 Neuendettelsau
GERMANY
Locations
Western Europe, Eastern Europe
Sandring Systementwicklung is located near Nürnberg, Germany.
Applications
All
Products

Microcontrollers

The following NXP products are supported:

Demonstration and Evaluation Boards

The following products are either developed by or supported by the consultant:
We developed of a modular test system for user-controlled execution of legally required or company specified work procedures and directives using an LPC2124 for measuring and controlling.
We have also created a small development platform for multiprocessing with several LPC210x and LPC2138 controllers and some analog and digital IO modules. It is a base development for an intelligent and autonomous control and navigation system for various kinds of robotics.
We have developed a very small, robust, and efficient real time operating system (RTOS) especially for LPC2000. The whole kernel needs less than 4kB flash and less than 400 Bytes SRAM. Please see nanortos.net-attack.de for more information.
We have also developed a serial flash loader tool for Linux (lpcflash4linux) for the LPC2000 family. It is freely available on the nanoRTOS homepage.
More Information

Background

Sandring Systementwicklung provides embedded hard- and software development, consulting, production, and compliance tests in cooperation with certified partner companies. In addition, we offer a small real time operating system named nanoRTOS, which has been especially designed for the LPC2000 family.

Disclaimer

NXP Semiconductors provides consultant information in an effort to support its customers through independent 3rd parties. NXP believes that the information presented herein is fair and accurate. NXP does not endorse or warrant a listed consultant's fitness for any particular purpose. You should contact the consultant directly to discuss your particular needs.
Standard ICs quick find
Standard ICs sections
See also