ProductsMicrocontrollersSupportConsultants

Consultants

Contact
MT-system Ltd.
Victor Lymar
13, Kalinina str.
St. Petersburg, 198099
Russia
Locations
Eastern Europe
Russia and CIS
Applications
Auto/Transport, Consumer, Financial, Industrial, Medical, Security, Telecom
Products

Microcontrollers

The following NXP products are supported:

Demonstration and Evaluation Boards

The following products are either developed by or supported by the consultant:
1. EVB-ARM-MT with LPC2106
HEADER BOARD IN DIL38 FORMAT. Dimensions: 50x28mm
2. EVB-ARM-MT with LPC2124; LPC2129; LPC2194
HEADER BOARD IN DIL57 FORMAT. Dimensions: 50x31mm
3. EVB-ARM-MT with LPC2138; LPC2148
HEADER BOARD IN DIL62 FORMAT. Dimensions: 61x61mm
4. Wig-MT JTAG adapter (10-pin) for EVB-ARM-MT with LPC2000
The Wig-MT JTAG adapter is a low-cost (MACRAIGOR WIGGLER COMPATIBLE) interface used in the design, debug, and programming of LPC2000 microcontroller based embedded systems. One side of the Wig-MT interfaces to the parallel (LPT) port of a host IBM compatible PC and the other side connects to an OCD (On-Chip Debug) JTAG port of the target system (used 10-pin connector specially for EVB-ARM-MT with LPC2000).
More Information

Background

MT-system Ltd. is the distributor of electronic components in Russia and CIS. The main direction of company is the promotion of NXP microcontrollers with technical and marketing customer support. MT-system has NXP-certified specialists to assist customers with component choice and hardware and software design. MT-system offers our own ARM debugging tools, as well as those from well known manufacturers including Keil and Olimex. We also offer software products (IAR Systems) and practical trainings for customers on the LPC2000 and LPC900 MCUs at the University Laboratory in St. Petersburg.

Disclaimer

NXP Semiconductors provides consultant information in an effort to support its customers through independent 3rd parties. NXP believes that the information presented herein is fair and accurate. NXP does not endorse or warrant a listed consultant's fitness for any particular purpose. You should contact the consultant directly to discuss your particular needs.
Standard ICs quick find
Microcontrollers sections
See also