ProductsMicrocontrollersSupportConsultants

Consultants

Contact
eSysTech — Embedded Systems Technologies
Douglas Renaux
Travessa da Lapa 96, cj. 73
Curitiba/PR 80010-190
Brazil
Locations
South America
Applications
Auto/Transport, Consumer, Industrial, Medical, Power, Security, Telecom, White Goods
eSysTech provides the following services and products to the embedded market:
  • Engineering of embedded systems: The development of hardware and firmware for ARM-based embedded systems, typically using an RTOS. Previous developments include the areas of telecommunications, energy, transport, industrial, and commercial automation.
  • X real-time kernel: Our RTOS was designed specifically for ARM microcontrollers. It is small and very efficient. The microkernel provides the basic functionality for concurrent programming while libraries provide support for TCP/IP, USB, FFS, and user interface.
  • Customized Products: We can develop and manufacture ARM-based embedded products that fulfill the requirements of your application.
Products

Microcontrollers

The following NXP products are supported:

Demonstration and Evaluation Boards

The following products are either developed by or supported by the consultant:
  • eSysTech provides evaluation boards for ARM microcontrollers. Our eAT55 board has been on the market for 2 years, and other boards are under development.
More Information

Background

Embedded Systems Technologies is a company focused on the embedded systems area. eSysTech provides both Engineering Services and Manufacturing of customized ARM-based embedded systems.

Disclaimer

NXP Semiconductors provides consultant information in an effort to support its customers through independent 3rd parties. NXP believes that the information presented herein is fair and accurate. NXP does not endorse or warrant a listed consultant's fitness for any particular purpose. You should contact the consultant directly to discuss your particular needs.
Standard ICs quick find
Microcontrollers sections
See also