![]() |
||||
|
||||
LPC3000 Evaluation BoardIntroduction
Nohau's LPC3000 Evaluation Board is an effective tool to develop embedded systems using the LPC3000 family of microcontrollers.
Developement for the LPC3180 is supported by the Seehau JTAG debugger, C compilers, and Real-Time Operating Systems.
Linux and μC/OS-2 RTOS have been ported to the evaluation board.
The evaluation board comes with a detailed user guide to help the user get a jump-start in LPC3180 development.
There is also an available option to upgrade the JTAG interface to add full-fledged trace debug functionality.
![]() Key Components
The development board has the following key components:
RTOS
Linux RTOS![]()
A Linux reference base port inlcudes:
The Linux reference base port comes with basic drivers typically needed in an LPC3180 system including:
A Linux package comes with an application note which explains the details on how to load the kernel and the accompanying software to the LPC3180 system.
Details on how to add user applications are also provided.
The LPC3180 does not have an Ethernet controller on board, but this application note shows how an Ethernet connection can be established over USB (using additional hardware).
μC/OS-2 RTOS
μC/OS-II is a highly-portable, ROMable, very-scalable, preemptive real-time, multi-tasking kernel (RTOS) for microprocessors and microcontrollers.
μC/OS-II can manage up to 255 tasks and provides the following services:
μC/OS-View is also ported to this board.
μC/OS-View is a combination of a Microsoft Windows application program and code that resides in the target system.
The Windows application connects with the target system via an RS-232C serial port.
The Windows application allows the user to 'View' the status of the tasks, which are managed by μC/OS-II.
A μC/OS-2 RTOS package comes with an application note that shows example code for using μC/OS-II on the NXP LPC3180 (ARM926EJ-S) processor which resides on the Nohau evaluation board.
DocumentationProducts
Supported Products
Click
More Information
Consultant Support
For additional support, customers may contact Tethermedia LLC for their services.
As a consultant, Tethermedia LLC provides a variety of services including application support and modifications to the base port to fit a specific hardware design based on the LPC3180.
Manufacturer Links
The Nohau LPC3000 Evaluation Board can be obtained by contacting the manufacturer.
Software Tool Links
A user can add their own applications and implement specific functions using the ARM-GCC cross compiler.
The compiler can generate image files that will run on LPC3180.
Terms of Use
|
||||