![]() |
||||
|
||||
NXP LED dimmer demoboardIntroduction
The LED dimmer demoboard demonstrates the capability of the I2C-bus to perform red/green/blue color LED lighting and mixing operations.
Two separate control cards comprise the demoboard:
![]() ![]()
The two control cards directly connect to each other without the need of external cables.
The keypad control card contains an NXP P89LV51RD2 microcontroller interfacing with a NXP PCA9564 I2C-bus controller to generate the I2C commands.
The microcontroller is programmed to allow the 16-key keypad to control the RGB color mixing, generate fun light patterns, and emulate battery status monitoring.
The LED control card accepts input from the keypad control card's keypad.
Power is supplied to the LED dimmer demoboard via the keypad control card by either an external 9V power supply or by a 9V battery.
The control devices on the demoboard are:
![]() ![]()
Firmware in the P89LV51RD2 microcontroller emulates a cell phone application.
It generates fun patterns and controls the brightness of a virtual display.
A battery discharge emulation with a visual charge status can also be performed.
The firmware is intended to show a specific application (cell phone), but the demoboard can be used and reprogrammed externally for any application that requires keypad control and LED lighting/color mixing.
Most of the code, written in C language, has been borrowed from the PCA9564 Evaluation Board (drivers and main interfacing files between the P89LV51RD2 and the PCA9564).
Only the upper layer files have been modified to implement the code specific to the LED Dimmer Demoboard.
Programming has to be performed using an external microcontroller programmer or the PCA9564 Evaluation Board Kit.
The default firmware in the P89LV51RD2 allows the user to:
The P89LV51RD2 can be programmed with any user-defined firmware.
The demoboard, however, does not have any built-in programming functionality, so the user must program the microcontroller with an external programmer or the PCA9564 Evaluation Board Kit.
For more information about the PCA9564 Evaluation Board, its drivers and code, refer to:
Support
Schematics
Source Code
Below is C language source code for programming the P89LV51RD2 microcontroller.
Please check back occasionally for the latest revisions.
Application Notes3rd-Party Tools
Below are links to third party software tools that you can use with the demoboard.
(Disclaimer: Access, use, and support of these tools is subject to conditions set by the third parties.)
Flash Magic
Flash Magic can be obtained from Embedded Systems Academy.
This software can be used to load the microcontroller with compiled hex files.
Please visit http://www.esacademy.com/software/flashmagic/ for more information, release notes, application notes, and to obtain the software.
Flash Magic is sponsored by
NXP Semiconductors.
Raisonance
The Raisonance 8051 Development Kit, from American Raisonance, may be used to develop, debug, and compile C language code.
Please visit http://www.amrai.com/amrai.htm for more information.
To obtain an evaluation version of the software which allows you to compile up to 4Kb of code:
The full development kit can also be purchased through the American Raisonance sales department.
More Information
Literature
Referenced Products
Click
Ordering Information
Part Number OM6279: NXP LED Dimmer Demoboard
The demoboard can be purchased from authorized distributors:
Links
|
||||