![]() |
||||
|
||||
Package markingsExample
Typical package markings include a pin 1 stripe and/or pin 1 dot, the company logo, and up to four lines of text, described below.
Figure: Package Markings Format Line 1
Product name including the package ordering code, for example, 74LVT2244D.
Note that commercial FAST products are marked without the N prefix, while industrial FAST products are marked with the I prefix. Line 2
Batch information for tracing lot history, for example, B38090ME.
Line 3
The first 3 letters contain codes to indicate the diffusion center, the assembly center, and the final-test center of the device.
The 4 numbers that follow indicate the assembly date code in the format YYWW.
The next character is an alpha-numeric code representing the revision of the silicon die contained within the package.
The final letter indicates the release status of the product as follows:
An example might be: HRn9744 F X.
Line 4
Optional text.
Truncation Note
On smaller packages, the markings may be condensed to two lines or even one line.
Truncation of characters within a line may also occur on small packages.
More Information
Links
|
||||